Using TPS3305-33DGNR to monitor 5V and 3.3VDC. We connect the MR pin to a push button switch for manual reset during development. This part includes a watchdog input which we do not use (left floating).
- What is the correct input state for Pin 7 for a design using the TPS3305 without a watchdog signal?
- Is there a pin-compatible replacement for the TPS3305 that does not have a watchdog input?
- Is there a more cost effective replacement for the TPS3305 that can be used to sense 3.3V/5V and provide an input for a manual switch with outputs similar to the 3305?
Jaden