I have a TPS3808G09 in my design which doesn't work properly. Its connections are like this:
VDD -> 3.3V
GND -> GND
Ct -> Open
MR -> Open
Reset -> Pulled up with a 10K resistor to its VDD (3.3V)
Sense -> To a 1.0V rail voltage
Since it's a TPS3808G09 it's supposed to toggle its Reset pin from Low state to High state when its Sense pin reaches a voltage more than 0.9V but in my case it doesn't ! It remains in Low state for good.
I don't get it. It's a simple Supervisor and Reset IC. Has anybody faced such a problem before?