The Ct pin of the TPS3808G01 can be connected to a ground referenced capacitor to set the user-programmable delay. What is the effect on the output if the ground referenced capacitor were to fail shorted? Is the delay limited to the 10 second maximum listed in the data sheet or is the /RESET output held low indefinitely after a reset is triggered?