HI
I saw a preview part TPS3421A.
Would you be able to share what is the main different between this A version and the original.
I have a customer looking for a TPS3421 with 15 sec t_timer, is there any suitable part?
Ivan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Ivan,
Sorry, the TPS3420 has the 12.5s option with TS tied to VCC you have a nominal 12.5s timer.:
Note the Iq, for the TPS3420 is nominally 350nA:
the max at 85C is 1.2uA and at 125 this can be as high as 3.4uA
The Iq you are showing is when the push buttons are pressed:
So normally the Iq is <<1uA but when the button are pressed, it increases as we start our internal timer.
I hope this helps.
Regards,