Hello,
The LP3470 reset time out period is 1ms(min), 2ms(typ), 3.5ms(max).
If the customer filtering the device by their test, is the time out period fixed on the following conditions?
In other words , can they filtering the higher reset timeout period device by their testing?
--------------
<Conditions>
Device : LP3470IM5X-2.63
Vcc=3.3V
Temperature range : 30C ~ 40C
Reset timeout period range : 3s ~ 9s
C1=3uF
--------------
<back ground>
Our customer would like to use this device with the time out period range as from 3s to 9s.
Thus they woul like to use 3uF for C1.
Time out period equation is the 2000 x C1.
I think that 2000 is the typical value and minimum value is 1000 and maximum value is 3500.
In this case, min and max value with 3uF are 3s and 10.5s.
Thus, they will filtering the device.
Currently , they concern that the timeout period is varied from their testing to after production.
Best Regards,
Ryuji Asaka