Hi,
I need a supervisory device to drive the active-low enable of the TPS75433 LDO to hold it inactive until the upstream 5V rail has come up.
The TPS3828 looks like it would work but the datasheet has conflicting information.
The Device Comparison Table shows the TPS3828 as having a RESET and /RESET pins where the RESET pin is open-drain.
However, the pin Configuration diagrams show it as having ONLY /RESET pin.
Which of these devices has the open-drain RESET pin?
Can I get a device that comes up with open-drain output and drives LOW after the VDD threshold and time out period have been satisfied?