Dear, All
A customer has been designed using the TPS3700-Q1.
TPS3700-Q1 data sheet of the output delay time has been described only typ value.
Please tell me the maximum value under the following conditions.
Temperature condition is -40 degrees or more and 110 degrees or less.
Other conditions are the same as the conditions of the data sheet.
Please tell me the value of Tphl and Tplh for the output pin.
There is no problem in the actual value.
Thanks, Masami M.