Hello,
I would like to sense the following voltage. However there is no voltage option for these power rail.
Thus, I would like to use TPS3702-Q1 with external resisotor.
Since the customer request the +/-1% accuracy, we couldn't use the TPS3700-Q1.
Can we use TPS3702-Q1 with external resistor?
If yes could you please let me know the calculation method and recommended resistor value?
(1) Rail : 1.03V, UV : 0.96V +/- 1%, OV: 1.04V+/- 1%
(2) Rail : 1.35V, UV : 1.3V +/- 1%, OV: 1.4V+/- 1%
(3) Rail : 1.25V, UV : 1.18V +/- 1%, OV: 1.31V+/- 1%
Best Regards,
Ryuji Asaka