Dear, All
A customer is a circuit using TPS3619, and a problem occurs.
Vout is not output at time when VDD did On/Off in short time.
They suspect that "Battery Freshness Seal" function of TPS3619 worked.
There is a question under conditions of "Battery Freshness Seal" function.
>3. Connect PFI to VDD (PFI = VDD)
They do not connect PFI to VDD.
The input voltage of the PFI is around 1.4V. (VDD=3.15V)
If other conditions match it then, does the "Battery Freshness Seal" function work?
Thanks, Masami M.