For a li-ion battery powered system, would it be recommended to use TPS389033 to monitor the input voltage of TPS62743 and enable/disable the operation of TPS62743 by connecting the __RESET pin of TPS389033 with the EN pin of TPS62743?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jon,
Assuming you want to use the the TPS389033 to monitor the li-ion battery (so the voltage does not go under the recommended V min) and you are operate the parts with in the operating conditions, you can control the EN input of the TPS62743 with the /RST output.
Remember to use a pull-up resistor on the /RST output of the TPS389033, since it is an open-drain output.
Best regards,
Nicolás
Hi Nicolás,
Thanks for your answer. Yes, I'm planing to add 1MOhms pull-up resistor on the /RESET output of TPS389033.
I have a slide switch for power on/off the device, should I connect the slide switch to the SENSE pin or to the /MR pin? The switch will drive SENSE to GND when off and to the VCC of the battery when on. I'm not sure if I should connect the on/off switch to /MR instead.
Any advice is welcome.