Hi Support,
What is the maximum pull down value allowed on the WDI pin (pin 4) to keep the watchdog enabled?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mark,
I saw this 1kOhm resistor in the design note, but it did not state that it is the maximum value.
So I would like to know based on what I can decide the pull down value. We tried to use 10kOhm resistor and it works.
So it must be a parameter such as port output current together with the Vil (input voltage low threshold) specification to define the pull down resistor.
Thanks.