Dear Sir
Please tell me TL7705CP-B, TL7705BCP and difference in TL7705ACP.
Now my customer is using TL7705CP-B.
Which is the better choice TL7705BCP or TL7705ACP.
Could you advice me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
These two device could essentially be used in a similar function, but there are some slight differences here and there:
One of the key differences is setting the time delay fro the response of the device: for the TL7705B the time delay is 2.6*10^4 *Ct whereas for the TL7705A is 1.3*10^-4 *Ct
The TL7705B was released later than the TL7705A so it is a relatively newer device and has some minor improvements.
For example the assertion time and deassertion time is improved for the TL7705B.
My recommendation would be to go with the TL7705B.
Best,
Michael