Is there a reason that the TLV803Z reset IC cannot be used as a 200msec LED blinker. My application is to show that a battery powered MSP430 application is running using an output port that switches at 1 Hz or 1 second 3.3v, 1 second 0v so that an LED would blink for 200ms every 2 seconds. The LED is connected through a resistor to the Reset output and the VDD input is connected to a MSP430 output.