This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Simple WDT device to reset every 12 or 24 hrs

Other Parts Discussed in Thread: TPS3813, TPS3851, TPS3823, TPS3828, TPS3820, TPS3824

Do you have something similar to TPS3813 but would have a longer timeout instead of 25 second.

We are looking at 12 or 24 hours auto watchdog reset but I think the small devices can't handle large capacitor value.

Also do you have something would do edge detection on WDI input and generate one-shot reset?

-Khoi

  • Khoi,

    The largest timeout we have is TPS3851 in the extended timing version with a 77 second watchdog timeout.

    We do have Watchdog Supervisors with a latched reset feature in which the /RESET will be latched low if the WDI is active (transitioning high to low) while /RESET is already asserted (low for /RESET). See TPS3820, TPS3823, TPS3824, and TPS3828.

    Please let me know if you have anymore questions!

    -Michael