Hello,
TPS3808-Q1's data sheet specifies on page 3 the range of 10 kΩ to 1 MΩ as a pull-up resistor of /RESET pin. Is it OK to use a different value? I assume it's no problem as long as the /RESET pin's sink current won't exceed its absolute Max rating of 5 mA or a voltage drop caused by IOH (/RESET leakage current) running through the pull-up resistor won't affect the pin's high level voltage.
By the way, how should I understand the description on page 3 "..., and allows the reset pin to attain voltages higher than VDD." I'm not quite sure what it means.
Best regards,
Shinichi Yokota