Hi,
We are using TPS3808G18DBVR IC for reset signal generation.
Our application is to connect the reset out signal from this device to 10# other input devices.
We have calculated total input capacitor at the input of the 10# devices is more than 100pF.
From TPS3808G18DBVR datasheet CL RESET =50pF.
Whether it is possible to drive the 10# devices by using TPS3808G18DBVR device ? then what is the tpd at RESET pin ?
Thanks & regards,
Divya