In the datasheet SLV219E Oct. 2010 of TPS3801K33DCKR there is a statement on Power-up reset voltage(2) and corresponding foot note says: “(2) The lowest supply voltage at which RESET becomes active. tr, VDD ≥ 15 us/V.”
I have nobody found which can explain what the statement “tr, VDD ≥ 15 us/V” means.
1. Could you please explain that?
2. Is there a minimum supply line ramp up rate requested?
3. If yes, shouldn’t it say ≥ 15 V/us and not 15 us/V?