Other Parts Discussed in Thread: TVS3300
Hi, Support team
Customer is looking for OVP fucntion solution on VBUS of Type-C/PD.
The below is my thinking solution.
OVP detection threshold is 24V. UVP function is no required.
Customer application has SINK / SOURCE mode as USB PD.
Do you have any technical concern at the above circuit during SOURCE mode?
And also, do you think that TPS3701 will clear ESD testing, IEC61000-4-2 standard?
If it is not cleared, please suggest some solution to me.
Thanks
Tamio