Hello
We are using the TPS3850 in a critical system that needs to test the functionality of the TPS3850 during operation.
I am using the 4% type so the voltage supervisory tresholds are 3.3V*1.048 = 3.4585V for the upper and 3.3V*0.952 = 3.1416V for the lower.
I will pull the nominal 3.3V sense pin with two FETs and resistors down to GND or to 5V to be able to test if the supervisory does make a reset.
Now when calculating the resistors I would like to get values so for example for the lower treshold I get a voltage at the sense pin of 3.1387V. This is only about 0.1% below the threshold. I would like the watchdog to make a reset then to pass the test.
Now in the diagrams of the datasheet the 1% and higher overdrive are shown and the reaction time seesms to increase exponentially the lower the overdrive. What are the overdrive timings for values below 1% overdrive? Does that mean at 0.1% under treshold the device will take seconds to reset?
Do you have any values/hints as to what is possible?
Thank you