I'm using LM57 as thermostat for Over temperature protection.
TheTOVER_N will remain active LOW when it i tripped.
I needed a single pulse reset to trigger the shutdown but it need to be released to HIGH or else the system will turn back on.
will TPS3422 /Reset go HIGH after the < 480ms of reset pulse, even if the button is pressed and held?
Thanks,
Khoi