What does the RESET timing diagram look like when the Vdd is applied long after the Vsense pin is applied.
Case 1: The Vsense is above the threshold as Vdd is applied
Case 2: The Vsense is below the threshold as Vdd is applied
Is the reset still delayed by the timer programming value?
Are the timer programmed values maintained in this situation? (20msec, 300msec, programmable)