Hello dear TI community.
Im using TPS3701 as a positive and negative voltage windows detector to enable or disable my LDO's.
But I've got some questions regarding my design.
I saw that negative voltate sensing could be done with TPS3700 (via Ti design note), I assume it's still valid for TPS3701?
Another question is my bigger concern, I've got two independent power lines (TPS7A4701 and TPS7A3301) which are powering some delicate opamp circuit.
Both comparators are measuring voltage and send enable singnal totally independent - which can make circuit unstable or even damaged due to power supply failure (only one regulator will work ATM).
I don't want to use only one comparator to feed enable singnal to both LDO's because it's totally pointless in my opinion (it will not solve my problem anyway).
So my question is - is there any way to combine two independent outputs from those comparator into one useful signal?
That signal will be later used to feed both EN pins of my regulators.
I just want to avoid situation when one voltage will be outside comparator range and LDO will be turned off and another one will be running anyway.
I'm looking to achieve mutual enable ONLY when both voltage from two comparators will be within range, if one voltage will be outside the window range then both regulators will be turned out.
If possible I want to stay with TPS3701 because solution size and cost and precision are really good with those chips.
And calculating everything is pretty easy too, I've got everything already calculated.
My circut is using two regs adjusted to +/- 18V, and thery feeded by +/- ~20-25V so both comparators are adjusted to monitor voltage within that range.
BTW I know that there some chips in the market which could be used to sensing both VCC and VEE voltages in one package, but they can be configured only as a UV or OV detector which not suit me in this case.
Thank you for help and time :)