in the datasheet of TPS3808G09DBVR,there is a note that “ a resistor from 40 kΩ to 200 kΩ must be connected between ct pin and vdd , i want to know if i use a 10k resistor as you see above ,What will happen?Will this cause the system to be stuck in uboot when power on,like pic below?
And this phenomenon does not happen often, there may be once every 100 power-ups.