• TI thinks resolved

UCD90910: UCD90910

Part Number: UCD90910

Hi,

We are using UCD 90910 in one of our application for Monitoring various power rails and Power Sequencing those power rails.

Active High signal from CPLD device is connected to UCD90910 (Pin No. 41- PWM4/ GPI4). When UCD gets High on this pin, it should turn OFF all the power rails.

Please let us know what are the ways to do it in Fusion Digital Power Designer.  

  • Genius 12505 points

    Hello

    Please refer the section 4.6 of the UCD90XXX Q&A document.

    if you want to use GPI to turn on/off rails, please enable the PIN SELECT RAIL STATE function, which is also covered in the mentioned documents.

    thanks

    yihe