• Resolved

UCD90320EVM-783: Internal temperature is not shown in the system monitor.

Part Number: UCD90320EVM-783

Hi,

The internal temperature is not shown in the system monitor of the Fusion software (7.0.11).

Does the UCD90320 has an internal temperature sensor or is the software not correctly displaying it?

Kind regards,

Ben

  • Genius 12185 points

    Thank you for pointing this out. UCD90320 has a internal temp sendor. we will work on this issue. meanwhile please select the external temp as a workaround.

    Thanks

    Yihe

    PS: Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

  • Genius 12185 points

    In reply to yihe:

    Hi Ben

    Actually this is not GUI bug, it is a setting issue. By default, the internal temperature range is default at 0-5C. please follow below snapshot to change the Max limit so that temperature can be properly plotted.

    Regards

    Yihe

    PS: Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!