• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » Sequencers » Sequencers Forum » TPS3808G09
Share
Sequencers
  • Forum
  • E2E Wiki
Options
  • Subscribe via RSS

TPS3808G09

TPS3808G09

This question is answered
Stephen Taranovich
Posted by Stephen Taranovich
on Jul 27 2009 22:31 PM
Intellectual1330 points

In a new design, I’m using a TPS3808 to supervise the voltage of an AA battery. If the voltage is below 0.9 V then the RST pin switches to another battery. In another circuit of the same project, the RST pin simply turns off a switching regulator and allows current from another power supply to supply the circuits powered by the converter just turned off. I selected the version 0.9 because AAs don’t have much more juice left below 0.9 V. In re-reading the datasheet I was not sure about the specs. In page 2 it shows TPS3808G09 with a nominal supply voltage of 0.9 V and a threshold voltage of 0.84 V. What is 0.9 V? Should I use the version G01 and add two resistors so I can have a thresold a bit highr that 0.84? Or should I live it with the 0.9 V version? Why is the threshold voltage so low in the G01 version (0.405 V)? The supervisory chips are powered by a 3 V power supply powered by a lithium battery which cannot be turned off.

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Scot Lester
    Posted by Scot Lester
    on Jul 28 2009 09:34 AM
    Verified Answer
    Verified by Scot Lester
    Expert5640 points

    There are four voltages relating to the operation of the TPS3808 (or any of our voltage supervisors).  There is the voltage applied to VDD of the IC which is used to power the internal workings of the chip.  Then there is the voltage rail you wish to monitor (this can be the same as VDD or not).  The voltage rail to be monitored is applied to a resistor divider which produces a voltage at the SENSE pin (Vsense).  When the voltage at the SENSE pin falls below the threshold voltage (nominal 0.4V for the TPS3808) then the reset output will be driven low.  

    For fixed voltage versions of a supervisor, the resistor divider is internal to the IC. The TPS3808G09 is typically used to supervise a 0.9V rail.  0.9V is the nominal voltage of the rail so we want the TPS3808 to assert reset low when the voltage on the 0.9V rail drops.  The internal resistor divider is programmed so that when the 0.9V rail drops below 0.84V, then the reset pin is driven low.  If you need reset asserted when the voltage rail drops below 0.9V then you would need to use the TPS3808G01 with an external voltage divider.

    Another important point here is the voltage on VDD.  The TPS3808 requires a voltage on the VDD pin between 1.7 - 6.5V in order to power the internal workings of the IC.  If you plan on powering the VDD pin from the battery, you will not have valid reset pin results below 1.7V.  The reset pin is forced low for VDD voltages between 0.8V - 1.7V.  The reset output versus VDD can be sumarized as follows:

    VDD RANGE                          RESET OUTPUT

      0-0.79V                                  High impedance, will float to whatever voltage it is pulled up to

    0.80 - 1.69V                            low impedance, forced low regardless of voltage on sense pin

    1.7V - 6.5V                              Normal operation, output determined by voltage on sense pin

     

    TPS33063808 vsense sense threshold VDD power rail valid output
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Stephen Taranovich
    Posted by Stephen Taranovich
    on Jan 07 2010 14:40 PM
    Intellectual1330 points
    TPS3808 diagram.pdf

    Customer came back and said:

    Attached is part of the circuit that includes the supervisor and the DC-DC switcher. As you can see I'm going to monitor the battery voltage. When it's 0.9 V - the battery is practically dead - I want the output of the TPS3808 U21 shuts down the switching power supply U23. Vcc is 3 V and generated by U23. When the RST pin of the 3808 is pulled down, it disables U23 and enables another power supply to guarantee VCC always be at 3 V.

    I wouldn't mind to have a 0.84 threshold so that I could squeeze a bit more juice out of the battery. The thing is that, even though the circuits powered by Vcc always draw very little current (less than 2 mA), once in a while they may need a bit more juice (about 20 mA). Therefore, at voltages below 0.9 volts there probably is little juice or no juice at all... and the RST would toggle up and down often when that short pulse of current is requested from the battery. It's not exactly a problem because the other power supply backs it up but I would prefer disabling U23 to have a clean switch from one power supply to the other.

     

    The TPS3808G09 has a Vit of 0.84 and the next is the G12. Is using two resistors the only way to get 0.9 V as the trip voltage? You said the G09 is typically used to supervise the 0.9 V rail. Do you advise me to use it as 0.9 V is its nominal supply voltage? Frankly, I would prefer a fixed value than having to use two resistors.

    I bypassed the sense pin with a 10 nF cap as the manual suggests and used a 390 nF for a reset delay time of approximately 2 seconds. I still have the option to pull Ct up with the 100 K resistor if I need a shorter (300 ms) delay. Therefore, I can use one or the other.

    As that 20 mA pulse of current will be less than 1 second, would the G09 be the correct choice? Looking at the timing diagram, it would switch back to the power supply U23 "long" after (1 second later) the voltage went above the 0.9 V, right?

    Any other ideas or suggestions would be welcome.

    Stephen Taranovich

    In a new design, I’m using a TPS3808 to supervise the voltage of an AA battery. If the voltage is below 0.9 V then the RST pin switches to another battery. In another circuit of the same project, the RST pin simply turns off a switching regulator and allows current from another power supply to supply the circuits powered by the converter just turned off. I selected the version 0.9 because AAs don’t have much more juice left below 0.9 V. In re-reading the datasheet I was not sure about the specs. In page 2 it shows TPS3808G09 with a nominal supply voltage of 0.9 V and a threshold voltage of 0.84 V. What is 0.9 V? Should I use the version G01 and add two resistors so I can have a thresold a bit highr that 0.84? Or should I live it with the 0.9 V version? Why is the threshold voltage so low in the G01 version (0.405 V)? The supervisory chips are powered by a 3 V power supply powered by a lithium battery which cannot be turned off.

    TPS3808
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • prashanth sujir
    Posted by prashanth sujir
    on Jun 05 2012 23:32 PM
    Prodigy10 points

    hi.. i am planning to use TPS3808 series supervisors.. my doubts regarding it are : 

    1> what if i try to supervise voltage rails above the threshold voltage For example : 3.3v rail connected directly to the sense pin of a "TPS3808g09 designed for 0.9V"

    2> what if i try and use a voltage divider circuit and monitor a 1.8v rail... Example... the voltage 1.8v divided to 0.9v at the sense point.. and fed the "TPS3808g09" instead of an adjustable Supervisor.. awaiting your valuable response..

    supervisor svs /MR DSP SVS regulator adjustable tsp3808
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Darwin Fernandez
    Posted by Darwin Fernandez
    on Jun 06 2012 13:45 PM
    Verified Answer
    Verified by Darwin Fernandez
    Genius11760 points

    Hi Prashanth,

    1) In the abs max table on page 2 of the datasheet, Vsense pin is not allowed to be greater than 7V. Placing a 3.3V rail on sense will not damage the IC. When the rail reaches below the threshold voltage, RESET will trigger.

    2) Remember, there is already a voltage divider internal to the IC. You can still use an external resistor divider from 1.8V to Vsense however, in order not to ensure no offsets or loading effects of the internal resistor divider, the current throught the external resistor divider must be at least 100x the current going into SENSE (1.7uA).

    Regards,

    Darwin

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use