Hi,
Looking at using the LM3881 in a slightly unconventional way - to sequence AC power using large solid state relays.
So, one question: How much current can the FETs on the outputs handle on a continuous DC basis? The simplest design would assert the INV pin and simply connect one side of some solid state relays to ground when powered on. Looking for 20mA-ish continuous. If the part cant do this I can easily get around it by adding a few FETs or something, but it'd be nice to keept it as simple as possible.
Thanks!