Hi Experts,
We are using UCD9090 in our design to manage reset and power sequence. The power sequencing is all fine with our protos. I am facing few queries with the ‘reset’ portion.
1. Is it possible to toggle the ‘System Reset’ using state change of GPI???
That is, I will change the value of a GPIO in the UCD9090 register through PMBus.
The reset should be toggled (assert and de-assert) and not follow the GPIO.
2. Can the RESET PERIOD of the Watch Dog be varied during run-time through PMBus?? Say, the Reset-Period
is normally 15seconds. Now, I want to reset the system, so I change the Reset-Period to 1second so that the
UCD9090 resets the system because of the WDT.
Awaiting your reply.
Regards