Hi,
We are using UCD9090 in our design to monitor power rails & to sequence it. We can able to power up all the power rails as programmed, but if any one power rail fails we would like to disable remaining rails.Please share the tested configuration file for below scenario, this helps to crosscheck our programming file.
Mon 1: 3.3V; GPIO 1: 3.3V modules enable
Mon 2: 2.5V; GPIO 2: 2.5V modules enable
Mon 3: 1.8V; GPIO 3: 1.8V modules enable
If any power rail fails, remaining two rail enable signal should be turn off the respective power modules.
Regards,
Lakshmi.