Hi,
I have designed two boards with UCD90120A (two of them in each board). On one board (Board #1) it works without any issues. However, in the second board (Board #2), Fusion digital power software is not able to find any UCD devices connected.
Differences between the two boards
1. In Board #2, some of the MON pins are floating
2. Supplies monitored/controlled are different
Please note that UCD Reset pin is asserted 'HIGH' always using an FPGA Output pin, and TRST is connected to ground with 10K resistor
Also I measure +1.8V at BPCAP bypass capacitor.
Please provide suggestions on debugging this issue