In our custom board we are using the same power supply design which is on AC701 evaluation board. As the power supply sequencers data flash need to be programmed, i am using the respective xml files downloaded from the AR#57452 to program the sequencers in our customer board through TI USB-GPIO EVM.
Iout Cal Gain=(voltage at the current sense pins/sensed current)=Rsense×Gain of the instrumentation amplifier.
for MGTAVTT rail; Iout Cal Gain=0.005×268.4=1342mΩ.
for MGTAVCC rail; Iout Cal Gain=0.005×134.3=671.5mΩ.
Why Iout Cal gain for MGTAVTT and MGTAVCC rails are given as 1428mΩ and 690 mΩ respectively in the project file, as the theoretical values are 1342mΩ and 671.5mΩ. Any response will be appreciated.
Regards,
Sudhamani