This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160 and UCD90240

Other Parts Discussed in Thread: UCD90240, UCD90160, PTH08T250W

Hello,

We consider to use UCD90160 and UCD90240 devices as power supply controller, particularly  sequencing and adjusting voltages power rails (with PTH08T250WAD power module) . The devices will be used to adjust power module voltage in closed-loop manner.

I would like to confirm the following question:

1. We have in our system outputs Sense+ and Sense- for 0.95V rail, which have to be monitored for closed-loop. 

a. Do you have any proved of-the-shelf solution for monitoring  differential signals w/ mentioned above parts? If yes please provide the suggested solution.

b. If the answer to previous question is "no" , Could you propose the part that can sense/monitor differential sense input?

c. What is the margining mode BW and how one can ensure stability of two control loops (one of power module and second UCD90*)? 

2. Except extra pins of UCD90240 (vs. UCD90160) is there any other conceptual difference?

Thank you very much,

Igal