I am using LM3880-1-AA IC to control power on and power off sequence for a xilinx FPGA.
I am controlling three DC-DC converter enable pins with the sequencer IC LM3880.
But as per the previous revision of the datasheet released in 2014 , there was no notes about dos and donts , which is added only in feb 2016 released datasheet.
As a result i have connected common 5V to both VCC and EN pin. With this i see that my power on sequence is still working fine , The three DC_DC converter outputs 1V>1.8V and 3.3V are fine.
But during power off all the voltages go off together simultaneously , can you let me know how i can achieve power off sequence properly.
The new datasheet clearly tells that VCC and EN has to be powered with separate voltages, but i have not followed it , as i was referring to old datasheet revision.
Regards
Akshay