Can you provide an example for 4 wires FAN controlling with UCD90120A ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Peng,
You can refer to Page 29 of UCD90124A to see detailed description of FAN control. For UCD90124A, we already have FAN control algorithm inside.
For UCD90120A, we don't have a FAN control algorithm in, But don't worry, you still can use UCD90120A to control FAN by your own methods. For example,
when your PMBUS host get the temperature, it can send PMBUS command to UCD90120A to change the duty cycle of PWM signal(PWM output signal you use to control FAN), then it can change the FAN speed . Hope it useful for you.
Best,
Luke
I have another question about Enable.
A rail is used as a power-supply enable only, the enable signal also configure voltage parameters (warn/fault...) in rail config .
I think that enable signal don't need to setted OVER fault, OVER WARN ,un warn,un fault ...and so on.
Hi Peng,
The enable signal also configure voltage parameters in rail config? what is this mean?
Do you mean you have two power rail? For example, One is 1V power rail, the second is 2V power rail. You want to use Rail #1 of UCD90120A to enable 1V power rail, and monitor 2V power rail (Voltage ,current, temp)?
If so, I think you can do that as long as your fault response logic make sense.
BR,
Luke