I am using 3rd party USB-I2C cable and unable to program UCD9081.
The 3rd party USB-I2C cable is below:
www.totalphase.com/.../
My procedure is as following.
(1) Specify my power supply sequence by UCD9081 EVM GUI.exe (Ver3.0.0.15).
(2) "File -> Save I2C Transaction" to generate UCD9081 I2C Transactions.txt.
(3) Program the UCD9081 as UCD9081 I2C Transactions.txt with the USB-I2C cable.
(4) Verify the configuration data as the pseudo I2C transaction code described in SLVA275B. Read data is the same as the Factory Default described in SLVA275B, so that I assume the programming failed (Erasure failed, too?).
Other information:
Register Read/Write seem successful.
- Reading 0x26 returns 0x40
- Reading 0x27 returns 0x55
- Reading 0x30 returns written value