Hi,
I have a UCD90120A in my system and occasionally it takes significantly longer to start the programmed sequences. I have a single GPI which controls when the GPOs are enabled.
The sequences always work eventually and I don’t need to connect to the Fusion GUI to make it work (i.e. I don’t think it’s gone into ROM_MODE)
I don’t have the brownout option enabled and there is no additional hold-up capacitance.
1. How often is the fault log written to the flash? The Fusion GUI says “periodically” – is there a figure?
2. How long does “reset and initialization take”?
3. The datasheet recommends a slew rate of 0.25V/ms on VDD - what happens if the system does not meet this?
Thanks
Stuart