I would like to use the LM3880 to sequence the enables to three linear regulators.
The three 100K feedback resistors are pulled up to VCC, same VCC is used to power up the three regulators. I have a problem regarding input power to the regulators, they seem to drop a bit below desired value.
Could using VCC, that pulls up the resistors, as an input voltage to the regulators be the problem?