I have bought UCD90SEQ48EVM evaluation module and installed Fusion Digital Power Designer 2.0.120 (BTW ver. 2.0.141 does not work on my Win 7: after 1 min. it is not possible to press "Write to Hardware" -> it is grayed even though I do changes).
After that I made a simple task. I want to sequence 2 LDOs with EN input and +5V outputs. I started with deleting all rails from 3 to 10 in 'Hardware Configuration' and let there stay only Rail 1 and 2 (Voltage is on MON1 and MON2 and Enable is on GPOI1 and GPIO2, respectively). In a 'Rail Config' tab I set +5V nominal voltage and Turn On Delay 250ms for both rails. On/Off Config is set to OPERATION only so I can switch it on/off when I give it a command (BTW it took me a quite long time to find out how to assert OPERATION in Fusion GUI. I do it via 'All Config' tab and Write to Hardware -> not documented!!! I still cannot find how to assert PMBus CONTROL signal via Fusion GUI!). There is no dependency set. Project file is attached.
Here is the problem. When I send OPERATION command to EVM only GPIO1 LED lights on, GPIO2 is still deasserted. I cannot make it set so only first LDO is enabled.
What do I do wrong?