This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160- Board not powering up after storing RAM to flash

Other Parts Discussed in Thread: UCD90160

Hi,

I am using UCD90160 on my board. I configured the voltage rails and the enable pins. And the voltage are coming up fine. This is monitored using the GUI and the USB interface adapter. 

But once the storing RAM to flash is done, and the USB interface adapter is disconnected from the board and then when the board is powered on, the voltage are not coming up, which are probed using a multimeter. 

Please help. 

Regards,

Rasif

The xml file is attached herewith.Partial Board_3V3_aCTIVE HIGH OPEN DRAIN_SEQUENCED.xml

The schematics is as attached below: