I am using UCD9090, when I use FUSION GUI to configurate UCD9090 the first time ,It cannot find the device
Then I use the UC3xxx/UC9xxx Device GUI Tool ,I can scan the part In ROM MODE ,but it indicates the part is UCD30XX
and PKG is 64 pins, not the actual pin number 48.
and I cannot run Scipter Runner to configure UCD9090, because the Scipter Run cannot scan the device in ROM MODE
or Program Mode. So what's happened,and How to write configuration of UCD9090 when chip is in ROM MODE