I see from the datasheet, that MON14-16 have input range of 0.2V to 2.5V.... whereas the other MON inputs are 0V to 2.5V. I have a few questions related to this:
- Why is this input range different for these 3 MON inputs?
- How does that translate to reported voltage, if the Vout scale factor is 1? If Vin < 0.2V, will it report 0V? If Vin = 0.4V, will it report 0.2V, or 0.4V?
- I have configured pin-52 (MON15) as a MON input to read voltage of an Analog Temp Sensor. I have not configured any over/under voltage responses, or anything else... I only read 0V on this MON15 input, regardless of what I physically measure at this input. Is there another step I must take, just to get the voltage to report for this rail?
Thank you.