Other Parts Discussed in Thread: TPS3702, , UCD9090A
Hello Team,
I am trying to find a sequencer for a customer who in their application want to sequence down based on voltage only. I had previously suggested a Supervisor instead like the TPS3702, but the customer was wondering do we have a sequencer similar to this product. Below is what the customer is trying to achieve :
" So I am trying to design power sequencing for an Arria 10 FPGA device. The FPGA could get damaged instantly if the wrong power down sequence occurs. Ideally, I would have a voltage supervisor monitoring the main input voltage. As soon as it detects a power loss, the FPGA will be put into a low power state and the power down sequence has to initiate. As shown below group 3 would be disabled as soon as a power loss is detected, group 2 would go down immediately after group 3 drops passed 10%, group 1 would immediately be disabled after group 2 dropped passed 10%. If group 3 takes too long to discharge and group 2 is discharged before it, the FPGA can get damaged.
I could add a long delay time and *assume the rails discharge, but then I have to have a huge bulk capacitance to hold the main rail up until sequencing is done properly. If the bulk capacitance is not large enough, the sequencer will lose power and not sequence the rails properly. That is why for me it would be ideal to sequence the supplies down based on voltage only.
I could as you describe setup fault slaves but how do I know when the rail that caused the fault actually reaches the 10% threshold?
The TPS3702 would actually be something I could probably use, but I am surprised that there are no digital sequencers that would provide similar functionality."
Would you'll know what could I suggest the customer to use in their application ?
Thank you for your time.
Sincerely,
Kishen