I'm working with a board that uses an UCD90120A as voltage monitor. Until three days ago the board was working fine, yesteraday when I powered the board up, all the voltage domains which the UCD90120A handles stays off. No power good output goes up and the PMB_Alert output is active all the time.
I've tryied to communicate with the IC by i2c, but I get only errors when reading. When listing all the devices on the i2c bus the UCD90120A seems to be with the right adress, but the registers queries are giving error.
The readings are being made in linux with i2cget and the connected devices query with i2cdump commands.
Regards,
Bruno