Dear TI team,
when setting up the "System Reset", the defined rail names are used rather then just the rail numbers (which is good !) but for the GPIs these are ignored. The already defined names from the "Hardware Configuration" for the GPIs should also be used here IMHO.
Best regards
Bjoern
P.S.: Using the names it would be even better, if the displayed name would not be cut off but rather there would be enough space so that the entire name string displayed on the "Hardware Configuration" page also would fit on the "System Reset" page.