Hi team,
Can my customer use different flag voltage for different channel and different from the VCC? Thanks.
BR
Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Can my customer use different flag voltage for different channel and different from the VCC? Thanks.
BR
Frank
The Flag outputs are open drain signal which can be pulled up with a resistor to any voltage as long as it doesn't exceed the recommended max voltage for the pin, which is VCC + 0.3V. All the Flag pins do not need to be pulled up to the same voltage as shown in the DS image below.
If a pull-up voltage greater than VCC + 0.3V is needed then you would have to include some interface circuitry between the Flag output and that voltage.