This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90240: SW tool

Part Number: UCD90240

Hi,

Do we provide material as below for customers?

1.     Sample code for UCD90240

2.     UCD90240 program tool, and how to program it.

 

Thanks!

 

Antony

  • Hi Antony
    I would recommend below two documents which help to ramp up the device quickly.
    www.ti.com/.../slua815 Q&A
    www.ti.com/.../slvub51 Fusion GUI Guide
    #1. The Fusion GUI does provide a example UCD90240 project file. if a UCD90240EVM is order, it comes with a example file
    #2. This is addressed in the above document. Basically,TI Fusion GUI provide GUI or command line tool to program the device.

    Regards

    Yihe