Hi,
I have a board with the UCD9090A sequencer that successfully sequence on and off the rails when I power the card on and off.
When I test a failure scenario that should sequence off the rails and sequence them back (re-sequence) the sequence off function ok but the device does not sequence on again.
I followed the instructions on "UCD90xxx Sequencer and System Health Controller PMBus Command Reference" document (slvu352f) section 10.25.2 "Re-Sequence" but still the re-sequence operation does not work.
I have 10 monitor supplies and a GPI that control the sequence on and off with the correct dependencies.
The setting of register MFR_SPECIFIC_44 "Miscellaneous Configuration Byte" is 0x88 which configures the sequencer to Resequence Continuously.
I can send any information that is necessary.
Please advice,
Best Regards,
Yossi