I have used the development board to create the programming file that I am using for the UCD90120A device on my PCB. However there is an issue with importing the configuration. I believe the reason for the issue is due to the fact that the device on the development board has address 101d and the device on my board has device 52d. Is there a way to change the address or to copy over the configuration file so I do not have to redo the entire thing for the device on my board?