Hello,
it is possible to deactivate the clock stretching at the UCD90160A?
regards
Christian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
it is possible to deactivate the clock stretching at the UCD90160A?
regards
Christian
Is that possible to modify i2c master?
It is not difficult to implement:
The master is required to read back the clock signal afte releasing it to the high state and wait until the line has actually gone high
Or you can try to slow the master clock from 400KHz to 100KHz or lower to see whether the communcation can be well established.
Regards
Yihe