Other Parts Discussed in Thread: TPS53319, TPS53355,
Hi,
For one of our modem design , we have multiple voltages to be sequenced for DSP, FPGA & power pc.
From 12v source , Buck converter TPS53319/TPS53355 will be used to generate lower core & peripheral voltages for DSP, FPGA and other devices.
We are planning to implement the Sequencing from external child card FPGA.
Since the sequencer (eg.UCD90160) will not be used and the sequencing will be done from ext.card ,
Is this correct if the Power GOOD out from the 1st device in the sequence can be fed as an Enable signal input to the next device and SO on in the sequence ?
plz suggest if there is any better alternative to this approach ?